Other Parts Discussed in Thread: LM5143
我在使用LM5143双相单输出结构来设计一个输入48V,输出为3~46V可调的一个电压源,该电压源为半桥驱动提供电压,平均电流为0.5A,瞬时电流可达4~6A。采用一个0~3.3V的模拟信号来控制FB点,从而使得输出电压VPP可以在3~46V可调。电路图如下

在空载调试过程中,FB的VPP_CTRL点接地,预期输出电压VPP应该是46~46.5V。但该芯片上电后无法正常工作,会在上电启动短时后工作马上停止工作,输出电压如下图所示。测得SYNCOUT脚输出的时钟波形也会相应地短时工作后马上停止。

做过如下尝试:
1.将VCCX直接接地或者外部5V供电电压,没有任何改善。
2.将SS的电容改成3.3nF或20nF,没有改善。
3.将EN使能电压从3.3V改为直接接Vin,没有改善。
3.猜测是上电时电流过大导致芯片停止工作,将两路的Vout和CS管脚直接用焊锡短接,后芯片变为在工作160ms后停止工作,输出电压阶梯式上升到15V左右断电,该值不稳定,每次上电后都不一样,偶尔直到10V,偶尔可以到20V,但是最终都会停止工作。输出波形如下图所示

同时,我发现SS点的输出电压会在上电后慢慢攀升,然后到200mV后就维持稳定。按照datasheet,该点电压应该可以达到FB+150mV。测得FB点的电压为90~100mV。
PG1和PG2因为没有使用需求,就直接通过100k电阻接地了。
测试中,VCC和VDDA均正常输出5V电压,在芯片停止工作后仍输出5V电压。