Other Parts Discussed in Thread: GPCRB, GPCCHEM
1. Let it stand at a low temperature of -40 ℃, and the temperature of the electricity meter can only be displayed at -30 ℃. Calibrated at room temperature.
2. Let it stand at a low temperature of -40 ℃, and the SOC of the electricity meter will decrease from 100% to 0%