客户LMZ14203已经批量,以前生产的都是Vout=5V±0.3V。近期批次出现Vout=5V超过理论误差范围,测试为Vout=5.5V以上。
分压电阻采用的都是1%精度的,100ppm的温升的,室温测试,没有长时间通电。
1、下图为批量原理图
2、下图为万用表测试输出电压5.5V
3、下图为示波器输出波形Vout=5V
下图为5V纹波
4、下图为PIN-6脚FB直流波形
5、下图为PIN-6脚FB电压
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
客户LMZ14203已经批量,以前生产的都是Vout=5V±0.3V。近期批次出现Vout=5V超过理论误差范围,测试为Vout=5.5V以上。
分压电阻采用的都是1%精度的,100ppm的温升的,室温测试,没有长时间通电。
1、下图为批量原理图
2、下图为万用表测试输出电压5.5V
3、下图为示波器输出波形Vout=5V
下图为5V纹波
4、下图为PIN-6脚FB直流波形
5、下图为PIN-6脚FB电压
Hi
纹波是否超过50mV?
确认一下反馈电阻的阻值是否正常?
这种异常多吗? 和正常品更换芯片,能确认到是芯片反馈基准出问题了吗? 同时从你FB波形看,纹波很大。
Hi
从你验证看,看起来是芯片问题。
奇怪的是,FB脚电压来自输出电压的分压,FB的纹波只会比输出纹波小很多,但是你的测试恰恰相反。