This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: 是否能用于输入24V,输出 -15V/2A 的应用上?

Part Number: TPS5430
Other Parts Discussed in Thread: TPS54560B, , TPS54360

客户有给应用,输入电压24V,输出电压 -15V/2A,从原理上看,应该要选择一个输入电压范围大于24+15=39V 的降压DCDC,所以我推荐了TPS54560B(输入电压65V).不过客户说他看到有其他竞争对手使用TPS5430 实现输入24V,输出-15V/2A 的应用(2A 会发烫,1.5A 稳定输出没问题),而且已经稳定量产好几年了。TPS5430 输入电压最大才36V,低于39V ,理论上应该是不能用的。客户咨询我们是否能借鉴竞争对手的这个电路设计使用TPS5430?最大36V输入电压是否不够,会有隐患?谢谢!