This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27541自动学习



附件是我配置的BQ27541的数据的GG文档,已经校准,校准没错。

为什么:

1、电池老化3次循环了Cycle Count还是0;

2、remaining capacity与FCC一直同步增减,是同一个数据;

急求大神指导。

bq27541g1.gg0128.xls
  • 1. CC Threshold = 7920mAh , 放出容量大于7920,mAh,count 才会+1,您放电的电池是多少容量的电池?

    2.Update status  = 0, 应该是阻抗跟踪算法没有使能,发送0x0021 到0x00中,使能IT,电量计才能正常计算。

    另外,您的ChemID也是默认的0128,如果需要提高电量计的精度,需要选择新的chemID,以及进行learning cycle.