This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我注意到该芯片的应用手册中有一个40W的TEC驱动电路,我有一点疑惑是TEC需要双向电流。使用buckboost是将TEC悬浮在输入输出电压之间,那么电流是否会从输出流入到输入内呢?这对供电源VIN的吸入电流提出了要求。其实,我更想知道具体的电流流向。
当输入比输出高时,电流流向是如下图所示吗?当输入比输出低,电流又该如何流动呢?
我现在可能需要扩展成驱动24V/15A的360W的TEC,那么就需要设计成是24V输入,5~48V输出,15A,将TEC悬浮在输入输出之间,满足TEC两端最大压差24V/15A,需要注意哪些地方呢?
HI
BUCK模式下 , HDRV1/LDRV1工作, 如你标识是低边MOS工作(Doff)时,当高边MOS启动时就是Don时。
这个芯片最重要的layout, 如果layout不好容易造成在输入和输出接近时,驱动出现不稳定。