各位设计师,你们好
我们设计一个POE供电输出5V的电路,目前POE的5V供电已经正常工作。现在,希望也能支持外部单电源供电。(poe后端电路支持范围为4.5V~18V,所以POE输出5V可正常工作)。
根据tps23753A芯片手册,电路设计为选用option3的方式,即:希望外部直接输入5V。
请问:是否可以如下图这样直接将外部电源正接到5V输出正?
若可以,那该option3的方式,RTN端和Vout的地端应该怎么处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.