This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

充电IC BQ24196 使用问题



请问 TI各位

我使用EVM,并在上面量测BAT脚位,只上5V电源,电池没接上,此时BAT可以量测到大约4V特电压,SYS有3.65V输出.

我参照EVM电路设计在我的板子上,也是只有上电, 但是BAT,输出电压却是0V,SYS有3.65V输出,电池无法充电.

电感有做过验证,结果还是一样,请问有什么地方是没注意到的吗?