This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用TPS7A3301实现-3V到-12V可调的系统

Other Parts Discussed in Thread: OPA340

我采用的输入电压为-15V,输出电压是-3V到-12V,原理图如下,其中运放我使用的是OPA340,DAC进过反向比例放大器后的电压是-2.7V到0V,这个电压经过一个30K的电阻后与FB管教相连

  这样的电路设计我在调试的时候TPS7A3301特别容易坏,我控制DAC的输出变化,让放大器的输出在-0.9V变化到-2.7v,这样几乎没调试一次,TPS7A3301都会坏掉,FB管教的电压稳不住,而且在SS管教居然会出现-14v的高电压,请问这个可能是什么原因导致TPS7A3301坏掉?