This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51772: 可多相并联4 Switch Buck-Boost变换器选择

Part Number: LM51772

我在为一个电池供电的系统设置稳压电源,电池电压可能会在9V~16V之间变化,我需要将不稳定的电池电压变换成稳定的12V向后级输出,输出电流需要支持到100A

我认为我需要使用如上图所示的4开关buck-boost模式的控制器,配合外部MOSFET来实现该功能

然而单独的VRM想要支持100A的输出电流是很难的,如果能够支持多相并联,则可以将每一相的需求降低,从而更易于设计

想请教一下Ti的专家,有没有支持2相以上并联的Buck-Boost控制器型号选择

或者不局限于这种做法,有没有任何别的方式来实现目标需求,将9V~16V的输入电压转化为100A的12V输出