This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295: 请求推荐一款锂电池电源管理芯片

Part Number: BQ24295


TI你好:

我正在设计一款低功耗产品(电池容量同时比较大,约6000mAh),需要一款单节锂电池充放电管理芯片。

需求如下:

能实现>3A的充电电流

输出系统电压固定为3.3V,断开外部电源时可以自动切换到电池供电,系统电流大于500mA即可

需要otg功能,仅使用一个usb-c接口,usb信号由微控制器提供(包括d+和d-两个信号,没有CC信号),输出电流最大不会超过1A

芯片本身的功耗不能太大

可以用多个芯片,但最好是用一个芯片来完成

谢谢!