Part Number: BQ24295
TI你好:
我正在设计一款低功耗产品(电池容量同时比较大,约6000mAh),需要一款单节锂电池充放电管理芯片。
需求如下:
能实现>3A的充电电流
输出系统电压固定为3.3V,断开外部电源时可以自动切换到电池供电,系统电流大于500mA即可
需要otg功能,仅使用一个usb-c接口,usb信号由微控制器提供(包括d+和d-两个信号,没有CC信号),输出电流最大不会超过1A
芯片本身的功耗不能太大
可以用多个芯片,但最好是用一个芯片来完成
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,推荐您看一下下面链接的芯片