Part Number: BQ4050
recovery delay 设置为:15S
在不连通信情况下测试:恢复延时为77.7S
连通信情况下测试:恢复延时为15S
两种状态 恢复延时相差 60多S。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,休眠状态恢复时间长与 Sleep:Voltage Time OR Sleep:Current Time参数有关
It looks like the device is also taking a current measurement when it wakes up every Sleep:Voltage Time OR Sleep:Current Time (whichever happens sooner). When the device exits sleep mode, it transitions to NORMAL mode. In normal mode, the current is sampled every 250ms, maybe this current is being accounted for current() continuous (see below)
Current() continuous means, the current needs to be sampled for a total amount of OCD:Recovery Delay.
For example, assuming Sleep:Voltage Time = 5s and OCD:Recovery Delay is 30s.
The current will be sampled after the device transitions to NORMAL mode every 5 seconds. But, the recovery requires a total of 30 sampled currents; and each sample current occurs every 5 seconds.
True Recovery Time = (Sleep:Voltage Time OR Sleep:Current Time) * OCD:Recovery Delay
To confirm the above, please set the voltage time to 3s and the true recovery should be 90 seconds.