我用的是单片机的IIC与bq28400通信,发现无反应。环境是无外部电源输入,插入两节电池(7.2V),BAT、DSG均为6.4V,VC1为7.13V,VC2为3.56V,REG27为2.71V,但smbus没反应,1、最有可能是什么问题导致?2、全新的芯片是否可以不通过smbus配置也可以正常充放电?3、用单片机的iic是否可以完成配置和读取??4、模拟smbus的话,芯片地址是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的是单片机的IIC与bq28400通信,发现无反应。环境是无外部电源输入,插入两节电池(7.2V),BAT、DSG均为6.4V,VC1为7.13V,VC2为3.56V,REG27为2.71V,但smbus没反应,1、最有可能是什么问题导致?2、全新的芯片是否可以不通过smbus配置也可以正常充放电?3、用单片机的iic是否可以完成配置和读取??4、模拟smbus的话,芯片地址是多少?