你好
我这边在使用TPS92682+TPS92520
TPS92682配置为CV,两相BOOST,合在一起带TPS92520
在配置TPS92682的时候遇到一些问题,请帮忙解答:
问题1:
CHxMAXDEN作用,开启和关闭有什么区别?
什么时候需要开启,什么时候需要关闭。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
我这边在使用TPS92682+TPS92520
TPS92682配置为CV,两相BOOST,合在一起带TPS92520
在配置TPS92682的时候遇到一些问题,请帮忙解答:
问题1:
CHxMAXDEN作用,开启和关闭有什么区别?
什么时候需要开启,什么时候需要关闭。
谢谢!
Hi
在表7-3下面有相关解释:
CHxMAXDEN:
0: Maximum duty cycle for the associated channel is disabled.
1: Maximum duty cycle for the associated channel is enabled.
主要是最大duty限制,这个会影响到输入电压的范围。
Hi
最大应该是到90%左右,到了最大duty就会限制,不会烧芯片,但是会导致输出异常。
再次感谢,我实际测试一下了,在实际项目中,我发现CHxMAXDEN:无论设置1或者设置0,测试SW节点最大占空比都在85%左右,再高了也上不去了,按字面理解,这个设置1,到底是限制占空比,还是不限制占空比?
CHxMAXDEN:
0: Maximum duty cycle for the associated channel is disabled.
1: Maximum duty cycle for the associated channel is enabled.
Hi
90%是典型值,在90%附近duty限制是正常的。
你好,90%的意思是最大占空比到了90%就会限制么,如果 CHxMAXDEN 设置为1,占空比到了90%,此时再增加占空比,占空比还会增加么,芯片会进行什么操作,输出会怎样?
如果 CHxMAXDEN 设置为0,到了90%,此时再增加占空比,占空比还会增加么,芯片会进行什么操作,输出会怎样?
谢谢
CHxMAXDEN:
0: Maximum duty cycle for the associated channel is disabled.
1: Maximum duty cycle for the associated channel is enabled.
HI
我是这样理解的。同时芯片最高的占空比也只有90%左右,一旦到达,输出会异常。