This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 数据读取异常和DCHG 异常关断

Part Number: BQ76952

Hi

我们在测试BQ76952的时候遇见了一些问题,还请帮忙解决下

1)在读取电流、电压时,由于数据进位导致读取的数据异常

如下是采集到的电芯电压

     

 

3328mV = 0x0D00

3072mV= 0x0C00

目前推测是电压由0x0D00变为0x0CFF的过程中,MCU在读取低字节(0x00)时,高字节的数据由0x0D变为0x0C,导致MCU读取的数据为0x0C00,与实际值0x0CFF相差甚远,请问这种问题该如何解决?

 

 

2)使用DCHGDDSG控制MOS管时,DDSG导通时会导致DCHG断开(使用的是FET_CONTROL子命令(0x0097)),请问这种问题有什么解决办法?

 

如下图所示,在DCHG导通时,导通DDSG会导致DCHG关断