我在TI产品手册目录里面查看,LM5013输出可以满足1.2V-95V;想问一下该款芯片是否可以满足;参考了LM5013设计文件,发现设置的输出电压一直不能稳定,并且在空载时有两个i芯片损坏,请问这是什么问题?
一下电路图

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照datasheet上描述这个芯片最大duty接近100%,所以最大应该是可以输出95V,但是你需要注意这是个降压芯片,要输出95V,输入最好是100V.
同时你需要注意这个芯片最大电压是100V, 所以你需要特别需要输入不能过过冲否者很容易烧芯片。
HI
也就是你改变滑动变阻器阻值改变输出电压,但是调整后的电压不能稳定下来是吗?
另外具体说明一下你的输入电压,此时的输出电压(最好是有波形),以及带的负载。