This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: In reverse mode, the output voltage (VAC) cannot be adjusted above 4V.

Part Number: BQ25756

Hi Ti team,

I ran into some problems while using BQ25756:

In reverse mode, the output voltage (VAC) cannot be adjusted above 4V.

When VSYS_REV is set over 5V, the IAC_DPM_STAT will be set: