This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在设计上使用了TPS48111Q1这款芯片,但是发现INP引脚输入高电平3.3V或者PWM信号,输出端GATE都没有信号输出。
如下是原理图设计,能否帮忙看一下,是否有什么排除建议,谢谢
Hi
将驱动上的电阻改为0ohm, 以及去掉D41/42,
另外确认一下EN脚的分压电阻?
EN引脚电压是2.4V;将驱动电阻改为0是指R132吗?另外问一下芯片4、5脚需要拉高到5V吗?
Hi
驱动电阻R131/2, R128/9可以都改为0ohm.
如果没有外部需求,FTL可以悬空,也可以上拉。
另外你芯片哪里买的?