This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25723: 搭配TPS656987DDH使用20V输入时无法充电

Part Number: BQ25723

各位专家好,

我使用TPS65987DDH+BQ25723搭建了充电电路,现在测试时发现在使用PD协商的20V输入时BQ25723无法为电池充电

已经测试过PD适配器协商15V输入时,可正常充电。我使用的电池的充电电压为8.4V,PD适配器支持最大65W输出

20V输入时无论设置充电电压为3.5A或者5A均无法充电。测试VDDA=6.069V,VSYS=6.69V

附件是我使用的TPS65987DDH的配置文件

1pd-change.pjt

请各位专家帮助解决此问题,谢谢!