This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: 搭配BQ25723的应用问题

Part Number: TPS65987D
Other Parts Discussed in Thread: BQ25723,

各位专家好,

我使用TPS65987DDH+BQ25723搭建了快充充电电路,现在使用PD适配器协商15V输入时,可正常充电;20V输入时无法充电。

使用的电池的充电电压为8.4V,PD适配器支持最大65W输出,ADCIN1 DIV=0.91

使用过程中发现以下问题:

1、使用15V输入充电时,只有先接入PD适配器让TPS65987DDH加载固件镜像后,再接电池,才能够进行充电。请问现在需要如何修改配置,能够在已接入电池的情境下,后接PD适配器能够正常充电?

2、按照问题1的操作开始充电后,电池充大概2~3分钟就会停止充电(BQ25723的看门狗已关闭)。此时重新快速拔插一次PD适配器,才能够持续充电,直到电池充满。请问这个问题该如何解决、问题原因是什么?

3、同时还发现在使用PD协商的20V输入时BQ25723无法正常为电池充电.该问题描述见BQ25723: 搭配TPS656987DDH使用20V输入时无法充电 - 电源管理论坛 - 电源管理 - E2ETm 设计支持 (ti.com)

以下文件为我所使用的TPS65987DDH固件:

PD sink 15V:

pd-change.pjt

PD sink 20V(BQ25723不充电):

3755.1pd-change.pjt

烦请各位专家帮助解决以上问题,不胜感激!