This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: TS2 问题

Part Number: BQ76952


在工作模式与休眠模式下,如果TS2一直被拉低,会有什么影响吗?

  • 您好,SHUTDOWN模式下,TS2 将通过弱上拉(~6Mohm)处于高电平闲置状态。要退出 SHUTDOWN,必须将引脚拉至 GND,然后将其唤醒。一旦发生这种情况,TS2将微弱地保持在0V附近。一旦发送 SHUTDOWN 命令,芯片会将 TS2 上拉至 5V。 如果TS2始终拉高,则无法退出SHUTDOWN。但是,如果TS2引脚始终短路至 GND,则芯片将永远无法进入SHUTDOWN状态,并且将始终保持在 DEEPSLEEP、SLEEP 或 NORMAL 模式。如果某些设计不使用 SHUTDOWN,则确实更喜欢使用此功能,因为它可以防止任何不需要的关闭。