此颗芯片是DCDC芯片,贴片后测试时,不带负载的情况下,污水泵口输出12V;带上负载时,污水泵的口输出变低,输出电压只有4V(正常情况下12V)!需要原厂分析下,芯片带载能力弱的原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
此颗芯片是DCDC芯片,贴片后测试时,不带负载的情况下,污水泵口输出12V;带上负载时,污水泵的口输出变低,输出电压只有4V(正常情况下12V)!需要原厂分析下,芯片带载能力弱的原因。
Hi
将输出电容加大一些,确认功率电感大于5A.
另外确认一下TPS54331能正常输出3A,? 而污水泵的最大瞬间电流需求是需要小于3A的。
Hi
你是指污水泵的电流需求是需要只有0.15A吗? 有没有测试峰值电流需求?
TPS54331的带载能力有确认吗?