Other Parts Discussed in Thread: LM5175
Hello,
我们用2个UCC27282DR实现4 N-MOSFET全桥buck-boost设计,UCC27282DR的VDD是12V输入,
在UCC27282DR的HI和LI都是低电平的时候,这个时候HO,HS都有7V左右的输出,这个是正常的吗?
这个是vout会有7V左右输出,这个是Q3的寄生二极管引起的输出7V吗?
如果这样怎么实现HI和LI都是低电平时,VOUT=0V输出?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
主控芯片是什么? 没有选用LM5175/6是因为电压不够是吗? 不过你可以参考LM5175/6的控制逻辑。
HI
我问主芯片,主要是怀疑控制逻辑,所以才建议你参照LM5175/6的控制逻辑。
Hi,
因为这个时候主芯片都没上来(是个小子卡),HI和LI都是下拉状态,就是没有控制逻辑,
相当于只有UCC27282DR本身只有VDD=12V,HI,LI是下拉,然后HS对地就有7V了.
Hi
HI和LI都没有输入,驱动输出应该是不会有电压的。
你可以在再通过信号发生器给信号再验证一下。