This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650332-Q1: TPS650332

Part Number: TPS650332-Q1


咨询关于PMIC故障开发问题,根据TPS650332-Q1数据手册的描述以及自己的理解总结以下几个问题,可以帮忙回答一下吗?

问题1:读取的值与手册不一致,无法确定我们读取的数据是否正确。

问题2:对PMIC寄存器的写入目前不能写入,是否有什么对应规则或者某些条件才能进行写入操作?

问题3:对于PMIC故障的开发,采用读取寄存器对应故障状态位作为判断依据,是否有相应的故障注入条件从而产生故障状态的变化? 目前在safetymanual文档中没有找到对应的故障注入方法。

 

问题1的背景说明:

目前通过IIC工具或者程序对芯片寄存器0h (PID)获取的值为0xda,寄存器1h(RID)获取到的值为0x59。而手册上提示的值分别为(PID)0xd0和(RID)0x09。

如下图一为 iiC工具获取,图二为手册上的数据。

图一:

图二:

问题三背景说明以下是部分故障检测寄存器说明