This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 相邻采集引脚的耐压

Part Number: BQ76952


你好,

规格书中只标注了Vcx引脚耐压为Vss+85V,但是Vcx(x) - Vcx(x-1)的最大耐压范围未看到相关注释,只看到推荐值为Vcx(x) - Vcx(x-1)=5.5V。

我使用4.2V的电池进行仿真,对偶数节电池V2和V4同时开启均衡时,参考如图,VC3-VC2=8.38V,VC5-VC4=6.29V,均大于Vcx(x) - Vcx(x-1)=5.5V的要求,因此我想知道Vcx(x) - Vcx(x-1)的最大耐压值能达到多少。