各位专家:
1.设计:输入范围20V~60V,输出33V/2A,电路原图图如下:
2.实际测试情况:输入38V~60V时,输出33V/2A工作正常;
3.实际测试情况:输入20V~38V时,输出33V时,最大电流1A工作正常;如果超过1A时,输出电压就会小于33V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位专家:
1.设计:输入范围20V~60V,输出33V/2A,电路原图图如下:
2.实际测试情况:输入38V~60V时,输出33V/2A工作正常;
3.实际测试情况:输入20V~38V时,输出33V时,最大电流1A工作正常;如果超过1A时,输出电压就会小于33V
HI
选择饱和电流更大一些的功率电感,并确认一下电流保护,包括sense电阻,以及layout。
最后就是确认layout,注意功率回路尽量小。
现在使用电感的饱和电流是8A,下面是Layout设计源文件,请帮忙看看,谢谢!
HI
轻载下如0.1A能否正常输出,如果可以的话,就要确认cs是否有较大noise,以及功率回路。