This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25638: 充电电流问题

Part Number: BQ25638


1、我们在做3.0V,3.6V,4.1V不同电压段在10-100mA充电时发现4.1V的电压要到40mA从能给电池充电,10-30mA VBUS输入有设定的电流值输入,电池端没有电流值。这个现象是什么机理造成的?

2、快充:我们ICHG配置的3200mA,3.0V进入快充后到3.5V,快充的电流都是3.2A,到了3.5V的时候,快充电流会跃进到3.4A左右,这个是什么引起的。