This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987DDK: device not load external confirguration from SPI

Part Number: TPS65987DDK


Above is the schematic for USB type.c power sink(UFP),dead battery mode,boot configuration is BP_NoWait, device configuration is Safe_Configuration.:

When X2 connect to type.c power sink,VBUS is 5V, LDO_3V3 is 3.3V,LDO_1V8 is 1.8V, VIN_3V3 is 0V


Issue: 1.device not load external confirguration from SPI, SPI_CLK, SPI_MOSI, SPI_MISO  no signal. The device performance not act as boot configuration:BP_NoWait, then checked datasheet, for unused pin need and SPI_CS  handle as below:

            1):GPIO1:Ground pin with a 1-Mohm resistor

            2):  I2C1_SCL: pull up to  LDO_3V3 with 10-Kohm resistor

            3):  I2C1_SDA: pull up to  LDO_3V3 with 10-Kohm resistor

            4):  I2C2_SCL: pull up to  LDO_3V3 with 10-Kohm resistor

            5):  I2C1_SDA: pull up to  LDO_3V3 with 10-Kohm resistor

            6):  SPI_CSZ:  pull up to  LDO_3V3 with 3.3-Kohm resistor

With all this, when power on,device not load external confirguration from SPI, SPI_CLK, SPI_MOSI, SPI_MISO  no signal.

Question:i) If device should act as:when power on,device not load external confirguration from SPI, SPI_CLK, SPI_MOSI, SPI_MISO  no signal?

               ii)If not, what issues can you found from my design?

               iiI)  I also try to change to below mode(R8 UN-mount,change R17 to 8K2):

                     

                     device performance still:when power on,device not load external confirguration from SPI, SPI_CLK, SPI_MOSI, SPI_MISO  no signal.

                    Can you help me for: If device should act as this

  • Hi

        TPS65987DDK方案比较复杂,而且需要程序控制,我这边没有硬件板子调试,也没有程序做起来就比较难。美国那边有这个芯片产品线的工程师对这个方案比较熟悉,他们也有板子可以调试,能更方便的帮到你们,所以才建议你们到美国E2E提问: https://e2e.ti.com/