在TPS65941212_FMEDA_version2p91_IEC62380文档中,Function and Diag Tailoring中对于MODULE-D1.1 BUCK1_DIGITAL的描述中:output voltage oscillation outside UV/OV range but inside detectable frequency range 的安全机制覆盖度是99%,请问能够检测到输出电压振荡超出UV/OV阈值的检查频率范围内是指多少范围?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在TPS65941212_FMEDA_version2p91_IEC62380文档中,Function and Diag Tailoring中对于MODULE-D1.1 BUCK1_DIGITAL的描述中:output voltage oscillation outside UV/OV range but inside detectable frequency range 的安全机制覆盖度是99%,请问能够检测到输出电压振荡超出UV/OV阈值的检查频率范围内是指多少范围?
Hi
震荡波形一般是没有频率的,我们通常只是用示波器观察其最大最小值。
Thanks Johnsin !
非常感谢您的回答,
我们在实际测试中模拟TPS6594X-Q1输出振荡的情况:将输出电感短路,测试输出电压产生振荡,通过示波器测试振荡的min和max值已经超过了芯片本身设定的UV/OV检测阈值,但是该故障并没有被芯片检测到,也就是输出的nINT信号仍然正常。
所以综合该芯片的FMEDA资料才对上述问题产生了疑问,怀疑是不是实际产生振荡的频率不在该芯片检测的frequency range内。
如果说芯片输出的纹波电压只要超过对应的UV/PV阈值,就会被芯片判断为故障的话那和实际测试的结果就不一致了,所以这是我的疑问,
希望您能帮忙解答,
添麻烦了,
非常感谢您!