This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5v输出的稳压器



我有一个噪声很大的5V电源,这个电源的电压也不是准确的5v,我想用一个LDO进行稳压并且降低噪声。我看到很多LDO的Vout=Vin+VDO   我这个电源电压大概有5.13v,有什么推荐的LDO吗?电流需要大于1A

  • HI

        如果你电源是5V, 而只是要降低噪声,再增加一个LDO,  最大输出是5V- Vdrop, 有可能会出现5V偏低的情况。

        你可以考虑增加一个LC用于降低噪声。

        如果没有电压降低的问题,可以选择TPS7A4501之类