This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: FCC偏大,FCC跟什么参数有关,为什么比PassCharge大很多?

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: EV2400

工程师你好!

     1.我想问下,FCC跟什么参数有关,为什么FCC比PassCharge大很多,例如电池包设计容量为10Ah,FCC一般为9.2Ah,但是Passcharge一般为9Ah,导致SOC放不到0,请问我该怎么优化调整,怎么样把FCC调整变小?

2.另外我想设置Avg P Last Run,这个参数该怎么设置合适的数值,我发现假如我设置的3200大,我通过EV2400修该后那么FCC就会变为3.6Ah,设置的比3200小FCC就有8.2Ah,这是为什么?假如FCC就会变为3.6Ah,经过冲放电静置后FCC会变化嘛?

3.User Rate-Pwr这个该怎么设置为合适的值

4.Reserve Cap-mAh、Reserve Energy,这个设置的值越大FCC就越小?我通过EV2400修该后FCC马上就会变小,假如经过冲放电静置后FCC会变化嘛?

5.在论坛说的TRM是哪个指导书可以附上链接嘛,感谢!

期待你的回复,感谢

x 出现错误。请重试或与管理员联系。