This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62595: 关于TLV62595输入欠压锁定的疑问

Part Number: TLV62595


工程师你好,

我们准备使用TLV62595,将输入5V转为输出3.4V,额定电流2A,峰值电流3A,

对于EN管脚,我将EN管脚上拉51K至输入5V,下拉16.9K至GND,因为EN的启动电压为1.0V,关闭电压为0.4V。

所以,通过分压关系可计算出,当输入5V上升至4.0V时,TLV62595开始输出3.4V,

但是如此一来,理论计算就得出,当输入5V跌落至2.4V时,输出3.4V才关闭(输入电压低于输出电压)。

请问:当理论计算的输入电压低于输出电压时,实际上芯片在输入跌落到多少V时,芯片就已经关闭了呢?

同理,若EN不分压,直接接在输入电压3.4V上时,芯片还是在输入上升到1.0V的时候就开启,并且在输入电压跌落至0.4V时才关闭么?

感谢。