This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL43xLI-Q1 2.5V基准芯片基端测量不准确问题




未加电容时:
1、在这种常规接法中,我们单独测量输出电压10V,非常准确;

2、我们单独测量2.5V电压,2.5V可能跳动为2.0V~2.4V,非常不准确。

3、我们同时测量上述两个电压,2.5V基准不准确,10V理论输出也同步减小(不准确),比例关系仍然存在。

添加电容后基准电压才稳定。

现在我的问题是:
1、我们原来的一个品牌的基准芯片可以准确测量且非常稳定,为什么这颗芯片不可以?
(我们设计时保证Iref驱动电流可以大于4uA;同时保证Ika大于1mA)

希望各位大佬能够解答!!!感谢!