Part Number: TPS929120-Q1
我在设计TPS929120驱动LED,遇到几个关于RREF电阻取值的问题:
1. Rref的选取有范围限制吗?1-50K的RREF范围都能出对应的电流吗?不能的话实际能满足的电阻范围是多少?我们测了小于3k似乎就不能出设定的电流了。但手册里说电阻可以1.58k。

2. 以下标注的电流精度,±5%的精度是全RREF都能满足吗?因为Datasheet里只标了RREF=8.45K 时候的精度,如下图。
![]()

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS929120-Q1
我在设计TPS929120驱动LED,遇到几个关于RREF电阻取值的问题:
1. Rref的选取有范围限制吗?1-50K的RREF范围都能出对应的电流吗?不能的话实际能满足的电阻范围是多少?我们测了小于3k似乎就不能出设定的电流了。但手册里说电阻可以1.58k。

2. 以下标注的电流精度,±5%的精度是全RREF都能满足吗?因为Datasheet里只标了RREF=8.45K 时候的精度,如下图。
![]()

HI
如你所说: – 高电流精度:电流为 5mA 至 75mA 时,精度 < ±5% – 高电流精度:电流为 1mA 时,精度 < ±10%
不需要考虑Rref电阻范围,如果你需要的电流较大如75mA, Kref=64, 那么此时电阻就是1.05kohm. 这个算是最小电阻了,精度是5%精度是可以的,当然选择1%精度更好。
HI
这个主要是需要板子来测试,我这边没有这个板子,如果你那边按照datasheet的推荐值测试出来仍然有问题(上述1.58Kohm),你可以在美国E2E上再确认一下,他们那边应该是有板子的。