我按照TPSM82901的图 7-3. Setable VO Operation Schematic推荐电路设计,R3=32.4k,R2=open。负载是20uF 10Ω。
其输出电压不能稳压。查看发现其开关频率达到7MHz,不是配置中的2.5MHz。不知道问题出在哪里。
CH1是VIN,CH2是VOUT, CH4是芯片电感上的波形。
明显的CH4的频率时7.35MHZ。CH2电压为2.1V,不是配置设定的3.3V。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
回答1:我换过芯片,特性有些变化,但还是不正常。
回答2:以下测试还是在用100欧姆负载进行。
R3 = 32.4K 2.5MHz出现了,我调节R3 = 75K 1MHz也出现了。说明MODE功能是完好的。
我对R2做了改动,接入一个94K的滑动变阻器。
从试验条件1、2中可以看出,PWM占空比调整功能是存在的。但目标电压不是规格书上的电压。这很奇怪。
从试验条件3中可以看出,当输入电压在5V~6.7V之间时,PWM占空比调整功能是存在的。但大于6.7V时,PWM功能失控。
从试验条件4可以看出,当输入电压在5V~10V之间时,PWM功能失控。
总结1:我这颗芯片的工作功能是有的。
总结2:在目标电压较低的情况下,输入电压较低时,可以稳压。但稳压的电压值与目标电压有所出入。
总结3:在目标电压较高、或输入电压较高时,PWM控制失控。几乎进入100%占空比模式。
猜测:我有种这个芯片的电压反馈功能不正常的感觉,或者目标电压不正常的感觉。
试验条件1:当R2=0Ω,即R2 = GND时,输入电压为5V和10V,输出电压为1.5V~1.6V。 但规格书目标电压时1.2V,与实际有些不符。


试验条件2:当R=8.87K时,输入电压为5V和10V,输出电压为1.28V~1.34V。 但规格书目标电压时1V,与实际有些不符。


试验条件3:当R=40.2K时,输入电压为5V和10V,输出电压为3.27V~8.1V。 但规格书目标电压时2.5V,与实际有严重不符。


其中在6.7V时,存在跳变。其占空比从53%突变为72%。这导致输出电压失去PWM调整能力。


试验条件4:当R=open时,输入电压为5V和10V,输出电压为4.17V~8.2V。 但规格书目标电压时3.3V,与实际有严重不符。