Part Number: LM5146
使用Webench生成的设计,使用贴在水冷板上散热,其它位置温度都不高,在50℃左右。
但主芯片温度有78℃,该问题如何解决。感谢!
webench.ti.com/.../51

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5146
使用Webench生成的设计,使用贴在水冷板上散热,其它位置温度都不高,在50℃左右。
但主芯片温度有78℃,该问题如何解决。感谢!
webench.ti.com/.../51

HI
78℃不算很高,如果你想再降低一些,需要注意如下:
1. 确认底部Powerpad是否充分与GND焊接,并扩展GND面积用于散热(包括如果是4层板,打孔中间层GND,用于散热)?
2. 适当降低频率。
3, 选择Qg更小的MOS.
Hi
一般不建议并联MOS, 选择电流稍微大一点的MOS都是可以的。