This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: 原理图CHECK及疑问咨询

Part Number: BQ25895


你好!

   原理图如下,请帮忙CHECK!

   疑问如下:

1、看手册理解在  VBUS接入的情况下,PMID是由Q1控制打开,VBUS=PMID(5V或9V或12V),SYS是由VBUS降压得到3.5V-4.5V;在未接入VBUS情况下,由VBAT升压得到PMID=5V,SYS=VBAT?

     如果是我上叙理解那样,是否可以保持关断Q1,不让VBUS=PMID,因为我的系统电源准备使用PMID的5V电压,如果VBUS充电时使用的9V或12V电压会烧坏我的系统电源(我的系统电源最高到5.5V)?

     如果Q1可以关断的情况下,在VBUS在接入的情况下,BQ25895是否可以一直保持5V输出来供我的负载使用?在VBUS不接入的情况下,PMID是不是直到VBAT<2.6V才不输出电压?

2、BQ25895芯片的配置是否是只用I2C接口即可,USB口可以不使用?

3、BQ25895芯片上的一些PIN脚电平是否可以使用3.3V的GPIO吗?(SDA/SCL/OTG/CE)