您好,我在芯片的IREF引脚串联了一颗10k欧姆的电阻接地,测试了单LED通道的输出电流在56mA左右,这是触发了芯片内部限流保护了吗?我该如何设计能正常输出最大35mA的电流?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在芯片的IREF引脚串联了一颗10k欧姆的电阻接地,测试了单LED通道的输出电流在56mA左右,这是触发了芯片内部限流保护了吗?我该如何设计能正常输出最大35mA的电流?
Hi
芯片应该损坏了,按照datasheet提供的公式10ohm,正常电流是7.35mA的电流,而实际电流异常到56mA.
如果是要35mA电流,Riref应该是2.1kohm。