This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: Cout 容值更換

Part Number: TLV62569


Hi All,

目前使用TLV62569PDRLR)設計,如下圖。


Vout=1.14V L=2.2uH&2.2A, C57(Cout)=22uF, 依datasheet建議,此Vout範圍建議使用222uF, 目前是使用122uF,請協助確認是否可以改成使用1*47uF?

 

Vout

L

Cout

Spec

0.6~1.2V

2.2uH

2*22uF

目前

1.14V

2.2uH,2.2A

1*22uF

Want New

1.14V

2.2uH,2.2A

1*47uF

謝謝