This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: 电池供电和USB供电如何切换

Part Number: BQ25606

想要实现:电池非满电情况下,插入VBUS可以给电池充电,SYS 由VBUS提供。

问题描述:先接VBUS,再接电池,可以正常充电。但是先接电池,再接VBUS无法进行充电。VBUS 5.2V  电池满电时4.2V 电池当前电源3.9V 

其他信息:SYS 负载190ma    电路图如下: