This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: 为什么需要先接BATT电池?

Part Number: BQ77915


Dears,

     您好!

     请问BQ77915 EVM 板说明上有提到需要先接BATT 这个电池,这是什么原因呢?

  • 您好,请参考下面链接的内容:

    Connecting the upper device cells to their VC pins before the VSS pins are connected could cause damage to the part.  With the proposed connection method, any of the other VSS and VC pins could be connected randomly.  This is a stressful situation even though the BQ77915 is designed with random cell connect in mind (as long as VSS is connected first).  Additionally, the BQ77915's recommended cell input resistors are relatively small, so this will not help to limit current into the VC pins. 

    Connecting cells from the bottom up helps minimize the voltage step applied to the board because the previous cell connected will charge the input filter capacitors, pushing up the cells above that are not connected.  The body diodes of the BQ77915's internal balancing FETs will also push up the unused inputs. 

  • HI

    请问规格书里面有相关的描述吗?

    我没有看到,是不是我遗漏了?

    谢谢!

  • 您好,请参考瞎买那帖子的内容

    e2e.ti.com/.../4835987