Part Number: TPS546C23
使用2块TPS546C23芯片并联/堆叠,理论上来说可以输出70A的电流,但是当负载达到20A的时候芯片就发生了电流报警,然后输出就自动关闭了
- 软件方面:读出芯片的 IOUT_OC_WARN_LIMIT 的值是37A,IOUT_OC_FAULT_LIMIT 的值是42A。
- 硬件方面:原理图依据推荐电路设计,参数没有改变,但是实际带负载能力不足。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS546C23
使用2块TPS546C23芯片并联/堆叠,理论上来说可以输出70A的电流,但是当负载达到20A的时候芯片就发生了电流报警,然后输出就自动关闭了

Hi
首先确认一下功率电感饱和电流足够大,其次确认layout上功率回路尽量小,这些都影响带载能力。
功率电感电流63A,在其他设计上有使用过输出30A没有问题,原理图是参考demo板的,上图是demo板原理图
Hi
直接按照评估板的操作来做,或者建议购买评估板对比下。
Hi
在美国E2E上问一下: https://e2e.ti.com/