This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23: TPS546C23: Overcurrent alarm occurs when current does not reach overcurrent threshold

Part Number: TPS546C23


Using two TPS546C23 chips in parallel/stacked (2-phase), theoretically it can output 70A, but when the load reaches 20A the chip has a current alarm, and then the output is automatically shut down.

Software: The value of IOUT_OC_WARN_LIMIT of the chip is 37A, and the value of IOUT_OC_FAULT_LIMIT is 42A.
Hardware: The schematic is based on the recommended circuit design, the parameters have not changed, but the actual load carrying capacity is insufficient.