This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650864: 需要配置才能输出电压给XCZU3EG供电吗,CTL和GPO如何使用

Part Number: TPS650864
Other Parts Discussed in Thread: TPS650861,

TI专家,你好。
我们公司目前正在基于XILINX XCZU3EG-1SFVA625I平台研发一款视觉产品,计划用TPS6508641供电方案。
1:我有一份XCZU3EG-SFVC784-1 + TPS6508641的原理图,我用625PIN的3EG是否可以完全参考其电源方案?即3EG的625PIN和784PIN型号,两者电源类型,上下电时序和电源功耗是否相似?
2:TPS6508641带IIC接口,是否必须EEPROM配置IIC才能输出电源,还是VSYS给电后它就给3EG供电了,那又如何区别MPSOC这么多型号的芯片上电时序呢,比如从3EG-7EG。
3:通过啥方法可以设置上电时序?
4:手册中分为ALWAYS-ON和FULL POWER两种模式,有啥区别呢?
5:CTL1-6和GPO1-4如何使用?是否可以通过CTL的上拉下拉来配置上电时序或者输出电压?请给出配置方法截图。
6:V5ANA引脚,内部带一个运放的作用是?我该如何给V5ANA供电?