This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2611: 关于LM2611输出电压的请教。

Part Number: LM2611


请问一下该器件能否输出-28V的电压?电流无要求,输入电压可以在0-28V。谢谢

May I ask if the device can output a voltage of -28V? No current requirement, the input voltage can be between 0-28V. thanks!