Part Number: LM2611
请问一下该器件能否输出-28V的电压?电流无要求,输入电压可以在0-28V。谢谢
May I ask if the device can output a voltage of -28V? No current requirement, the input voltage can be between 0-28V. thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2611
请问一下该器件能否输出-28V的电压?电流无要求,输入电压可以在0-28V。谢谢
May I ask if the device can output a voltage of -28V? No current requirement, the input voltage can be between 0-28V. thanks!
HI
建议你不要用LM2611, 如果你最大输入28V,输出要-28V,建议用超过56V的降压芯片来做,其带载能力需要对于Io/(1-D), D=Vo/(Vo-Vin)。