This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: 触发ASCD放电短路保护,导致无人机断电坠落。

Part Number: BQ40Z50


log0322-zhaji.gg.csv

无人机发生了空中断电坠落的情况,目前排查原因。

无人机电池为4s电池串,采样电阻1hΩ。

附件为出现事故后电池gg.csv文件。

请教以下问题:

1、gg文件显示,电池完成了6次循环,事故应该是第6次或者未完成的第7次循环,而最后一次发生ASCD EVENT是在第4次循环。因此是否可以认为本次事故与ASCD保护断电无关?

2、设定的放电短路保护电流应该是最大的,200A,而log记录的最大放电电流为10A,为何会触发ASCD?

3、ASCD如何关闭?

期待您的回复,谢谢。