该板还有2颗TPS563200分别用于12V/5V和12V/3.3V,但他们都工作的没有问题,这不是第一次使用TPS563200了,但第一次碰到这样的问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电源芯片一般不建议直接插电(热插拔),原因是因为启动瞬间会有高压震荡,可能损坏芯片。如果是必须有插电操作,需要在输入增加热插拔电路,或至少增加TVS管保护一下。
后来我又测试了一下,一开始只在输出5V侧增加了型号ESD5451N-TP的TVS,插入USB后,12V输入就对地短路了,然后在输入12V侧又增加了型号PESD12VL1BA的TVS,相当于输入输出都增加了TVS,插入USB后,输出侧对地短路,并且尝试了两次,都是一样的情况。
然后换成了型号TPS563201的芯片,尝试插拔USB数十次,并没有发生故障
还有个问题是,我的板子是有两部分5V供电的,主供电和USB供电两部分,两个部分的5V供电用了两片TPS563200,之前都是用主供电的5V通过一个0欧电阻给USB部分供电的,像这样也一直没问题。后来把0欧电阻去掉,单独把USB部分补上之后,就会有这样的问题
下面是原理图和USB供电部分的布局


HI
空载下,做启动测试(按你现有的测试), 看一下Vin的电压波形看是否有较大上冲? 如果不大,逐步增加负载看看?
测试时,可以输入电压小一些,测试从6V开始,最好是从板子上给电压。