Other Parts Discussed in Thread: LM25184
使用LM25184这颗料,有两个应用需求输入电压是6-40V,输出的两个需求分别是输出3.3V 和12V,负载功率8-12W。这样的应用场景使用L:M25184是否OK.
如果6V的输入时,12V输出时,输出电流最大值是600ma,功率在7.2W,可能存在风险?
如果6V输入时,3.3V输出的最大电流能到多少?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用LM25184这颗料,有两个应用需求输入电压是6-40V,输出的两个需求分别是输出3.3V 和12V,负载功率8-12W。这样的应用场景使用L:M25184是否OK.
如果6V的输入时,12V输出时,输出电流最大值是600ma,功率在7.2W,可能存在风险?
如果6V输入时,3.3V输出的最大电流能到多少?

Hi
1. 可以的。
2. 没有问题。
3. 可以借助webench,3.3V最大可以输出超过2A.